Despread Code Channel (W-CDMA(3GPP)/HSPA)
0 (See W-CDMA(3GPP) Standard Setups/Presets Table.)
0 to (Spread Code Length -1)
is used to specify the channel used for the Despread Channel trace data results.
Use the Copy Mkr To Despread Channel marker feature to automatically enter the , , and settings.
See Also
Available Chip Rates, Symbol Rates, and Spread Code Length