Decode Channel Type (W-CDMA(3GPP)/HSPA)

Menu Path: MeasSetup > W-CDMA(3GPP)/HSPA Demod Properties > Channel/Layer tab

Default: None (See W-CDMA(3GPP) Standard Presets Table.)

Decode Channel Type specifies the despread channel type for decoding the Despread channel.

Downlink

For Downlink, the available Channel Type choices are:

Downlink Decode Channel Type is only available with a Spread Code Length of 128 and a Code Channel of 96. The DTCH channel is only active when Measurement Interval is set to a multiple of 30 slots.

When Downlink Decode Channel Type is set to DTCH, a DTCH CRC Cyclic Redundancy Check data field appears in the Despread Channel Syms/Errs Table, which reports a PASS/FAIL CRC decoding result.

Uplink

For Uplink, the available Channel Type choices are:

Uplink Decode Channel Type is only available when Measurement Interval is set to a multiple of 30 slots, with Enable HSPA Analysis selected and a Spread Code Length of 256.

See Also

Channel/Layer tab - W-CDMA(3GPP) Demod Properties

W-CDMA(3GPP) Demod Properties