IQ Branch (W-CDMA(3GPP)/HSPA)
I (See W-CDMA(3GPP) Standard Presets Tablel.)
The parameters (, , and) selects which branch data is being analyzed. Select measurement data for either the "I" branch, "Q" branch, options or "IQ" the composite I and Q branches. View the data results in the Despread Channel Syms/Errs Table trace.
- "I" option: Selects I branch data results
- "Q" option: Selects Q branch data results
- option: Selects IQ composite branch data results
This selection is available only for the Direction.
Use the marker feature (for example, the trace marker location) to automatically enter the , and setting.
See Also