tHS-DPCCH (WCDMA(3GPP)/HSPA)
Code Location = S256(1):I
Value: 0 x256 Chips (See W-CDMA(3GPP) Standard Setups/Presets Table.)
: Value: 0 to 10
specifies the time offset (muliples of x256 chips) of the HS-DPCCH Dedicated Physical Control Channel (uplink) for HS-DSCH slot within the code channel. The HS-DPCCH Dedicated Physical Control Channel channel is an uplink physical channel with fixed spreading factor 256 and can only occupy the following four possible code channel and branch locations; 1(I),32(Q),33(Q) and 64(Q).
Use the following properties to specify the HS-DPCCH time offset:
- : Select one of the available code channels
- (SF 1) Spreading Factor, or 2) service flow: A unidirectional flow of medium access control (MAC) service data units (SDUs) on a connection that is provided a particular Quailty of Service (QoS). 256, Code Ch 1, I branch)
- (SF 256, Code Ch 32, Q branch)
- (SF 256, Code Ch 32, Q branch)
- (SF 256, Code Ch 32, Q branch)
- : Specifies the time offset in multiples x256 chips. The offset value can only be changed for the channel measurements and not for the composite measurements.
The Despread Channel ( and ) must equal the for the offset to be selectable.
See Also
Channel/Layer Tab - W-CDMA(3GPP)/HSPA Demod Properties
W-CDMA(3GPP)/HSPA Demod Properties