Scramble Offset (W-CDMA(3GPP)/HSPA)
0 (See W-CDMA(3GPP) Standard Presets Table.)
0-15 (Downlink only)
Scramble Offset specifies the scramble code offset. The must match the scramble code offset of the signal being analyzed in order for the VSA to lock to the signal.
This parameter is only used for signals.
See Also