Synchronization Start Slot (W-CDMA(3GPP)/HSPA)
Automtic (See W-CDMA(3GPP) Standard Setups/Presets Table.)
: 0 - 14
manually specifies which slot (0-14) is analyzed. The VSA demodulates and analyzes the signal on a slot by slot basis within the acquired data result length. With this parameter the VSA can be forced to measure and analyze a particular slot of interest.
Selected (default): Sets the VSA to auto sync slot measurement mode. The VSA will automatically sync to and begin the measurement analysis on the first fully captured slot in the data acquisition result length.
Cleared: Sets the VSA to manual sync slot measurement mode. The VSA will sync to and perform the measurement analysis on the specified slot within the acquired data result length.
The channel measurement summary results in the Despread Channel Symbol Table and the composite summary results in the Composite Error Summary Table can be viewed for the specified slot.
See Also