Inst CDE Composite (W-CDMA(3GPP)/HSPA)
trace shows the instantaneous (non-averaged) Code Channel power error data for the composite signal. trace data is the non-averaged CDE Composite trace data. (See CDE Composite Trace Data).
is not affected by averaging.
MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Measurements ( only): There is a seperate trace result for each measurement Antenna (x).
See Also