Inst CDP Composite (W-CDMA(3GPP)/HSPA)
trace shows the Instantaneous (non-averaged) measured code channel power for the composite signal. It is the non-averaged CDP Composite trace data.
trace data is not affected by averaging.
MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Measurements ( only): There is a seperate trace result for each measurement Antenna (x).
See Also