Inst CDP Layer (W-CDMA(3GPP)/HSPA)

Inst CDE Layer trace shows the measured instantaneous (non-averaged) Code Channel power for all active code channels (Walsh Code Number) within the specified code layer (Spread Code Length). It is the non-averaged CDP Layer trace data (see CDP Layer trace data).

Inst CDP Layer trace data is not affected by averaging.

MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Measurements (Downlink only): There is a seperate trace result for each measurement Antenna (x).

Selecting a Code Layer

Select the desired code layer by selecting the Spread Code Length in the CDP-Layer Spread Code Length text box (Analysis > W-CDMA(3GPP)/HSPA Demod Properties > Channel/Layer tab).

See Also

CDP Layer Trace Data

Available Antenna CDP Trace Data

About Trace Data (W-CDMA(3GPP))