Despread Syms/Errs (W-CDMA(3GPP)/HSPA)
When Demodulation is enabled, selecting trace data shows the channel symbol table. The symbol table provides the signal quality error information and the binary bits for each symbol for the specified Code Channel and code layer (). The bottom half of the display shows the symbol data bits and the upper half shows the error summary data.
For more information see the following topics:
There is also composite error summary trace data (), which provides the signal quality error summary information for the composite signal. (See About Composite Error Summary Data)
How to Make a HSPA+MIMO Despread (x) Trace Data measurement
To learn how to use the Despread Traces parameter to make a Despread (x) Channel Trace Data measurement, see HSPA+ MIMO Overview - Despread (x) Trace Data.
See Also