Inst Err Vect Spec (802.11b/g DSSS/CCK/PBCC)
When Digital Demodulation is enabled, the trace shows the instantaneous spectrum of the Error Vector Time trace. This is the non-averaged Error Vector Spectrum trace data.
The VSA's digital demodulator removes carrier-frequency error. Therefore, in the display, add the carrier-frequency error to marker readouts to obtain exact frequency information. The carrier-frequency error (Freq Err) is shown in the symbol table.
The center frequency and span for is identical to IQ measured spectrum. For details, see IQ Meas Time.
See Also