From SIG Symbols (Result Length) (802.11n/ac/ax/be/bn)

When Result Length is set to From SIG Symbols, the demodulator compares the information detected within the L-SIG Non-HT SIGNAL field, HT-SIG High-Throughput SIGNAL field, or VHT very high throughput (VHT) physical (PHY) layer protocol data unit (PPDU):A PPDU transmitted using the TXVECTOR FORMAT parameter equal to VHT.-SIG field to the Maximum Result Length parameter and uses the smaller value as the measurement result length.

This setting does not apply to 802.11ax/be (HE) formats.

See Also

802.11n/ac/ax/be/bn Demod Properties

Result Length

Time Tab