Maximum Result Length (802.11n/ac/ax/be/bn)

The Maximum Result Length value is shown in the text box to the right of the Automatic and From SIG Symbols parameters and specifies the maximum number of symbols that can be included in the measurement result length when Automatic or From SIG Symbols is selected.

See Also

Automatic (Result Length)

Result Length Parameters

Result Length

Time Tab

802.11n/ac/ax/be/bn Demod Properties