Subcarrier Spacing (802.11n/ac/ax/be/bn)
The parameter specifies the subcarrier spacing of the 802.11n/ac signal. The subcarrier spacing must match the input signal value. However, the value can be adjusted for troubleshooting purposes or to match a custom or nonstandard subcarrier spacing. The default is 312.5 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second)..
is only visible for the 802.11n/ac standard formats. For 802.11ax/be (HE) standard formats, see Subcarrier Spacing (Pre-HE) and Subcarrier Spacing (HE).
See Also