Subcarrier Spacing (HE/EHT) (802.11n/ac/ax/be/bn)

The Subcarrier Spacing (HE/EHT) parameter specifies the subcarrier spacing of the 802.11ax/be signal's symbols for the HE/EHT STF, LTF Long Training field, and data.

Subcarrier Spacing (HE/EHT) is only visible for the 802.11ax/be standard formats. For 802.11n/ac standard formats, see Subcarrier Spacing.

Default: 78.125 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second)..

See Also

Advanced Tab

802.11n/ac/ax/be/bn Demod Properties