Automatic (802.11n/ac/ax/be/bn)
Data Subcarrier Modulation Format
When is selected, the VSA uses the IQ data detected within the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. burst to automatically determine the data subcarrier modulation format for each user.
See Also