Manual (802.11n/ac/ax/be/bn)
Data Subcarrier Modulation Format
When is selected, the data subcarrier modulation format can be manually specified. The VSA ignores the format determined from the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. burst and sets the expected modulation format for all streams to the modulation format specified in the text box.
See Also