Compression Mode RU Settings (802.11n/ac/ax/be/bn)

For 802.11ax and 802.11be multi-user case scenarios, different users are designated to different spatial time streams when the compression mode is on (Sig B Compression Field selected).

802.11ax/be Standards (Except 802.11ax 80+80 MHz)

The following rules apply to all 802.11ax/be standards except 802.11ax 80+80 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second.:

Compression Mode RU Settings is comprised of a User Number and an Edit RU button. Clicking Edit RU opens a Multi-User Settings Editor that is specific to compression mode.

User Number - Displays the configured User Count.

Edit RU... - Opens a Multi-User Settings Editor that is specific to non-compression mode.

802.11ax 80+80 MHz Standard

The 802.11ax 80+80 MHz standard only supports one measurement channel per each 80 MHz segment. Therefore, the number of transmit chains (Ntx) is fixed to 1 and only one user exists in each 80 MHz segment. Since there are two single-user segments, the Multi-User Settings Editor does not apply and is replaced with a simplified Seg n Settings dialog for setting the MCS modulation and coding scheme for each segment.

See Also

Format Tab

802.11n/ac/ax/be/bn Demod Properties