Spectrum (802.11n/ac/ax/be/bn)
The trace is the averaged Instantaneous Spectrum display, as shown in the following block diagram. If averaging is off, the and displays are identical.
The trace has the following characteristics:
- It is derived from pre-demodulated time data.
- It is averaged
if averaging is ON and the average type is rms, rms exponential, or peak
averaging.
If averaging is ON, a scan is not included in the average if any of these conditions exist: Pulse Not Found, Sync Not Found, Carrier Unlock, or certain DATA? conditions.
VSA signal flow (see Digital Demodulation Block Diagram):
See Also