CDF (1xEVDO)
shows the cumulative distribution function for the data in the Measurement Interval. shows the probability that the voltage of a random data sample (x) will be less than K volts, where K is a value on the x-axis.
CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X.(K) = Probability(x £ K)
The CDF is computed by integrating the (Probability Density Function).
This trace can be useful in designing an amplifier for a particular type of signal. For example, for an amplifier that saturates at 212 mV, place a marker at 212 mV to find what percentage of the time the signal is below the saturation level.
This trace will continue to accumulate data until the measurement is restarted.
For more information, see the CDF trace topic in the Reference.
See Also