|
(Read-Write) Set the value of the Auto Sync Limit Lines that the User may access from the Limit [8] menu in Channel Scanner when Scan Mode is EMF Custom List. |
|
|
Relevant Modes |
Channel Scanner ONLY when Scan Mode is EMF Custom List. |
|
Couplings |
If Auto Sync Limits is ON: Recalling a limit line file OR editing the limits will overwrite the limit settings in the EMF Custom List.
If Auto Sync Limits is OFF: the values in the EMF Custom List will remain unchanged when editing the limit line or recalling a limit line file. |
|
Parameters |
|
|
<bool> |
Auto Sync Limit Lines state. Choose from: 0 or OFF - Do NOT sync the limit lines with EMF Custom List when Editing or Recalling limit line data. 1 or ON - Do sync the limit lines with EMF Custom List when Editing or Recalling limit line data. |
|
Examples |
CALC:LIM:SYNC ON |
|
Query Syntax |
CALCulate:LIMit:SYNC? |
|
Return Type |
Boolean |
|
Default |
1 or ON |
Last Modified:
|
26mar2024 |
New command (A.13.00) |