:CALCulate:PARameter:COUNt <n>

(Read-Write)  Sets and returns the number of traces on the screen. All traces are displayed in separate windows. Use DISPlay:WINDow:SPLit to set overlay (traces in same window) configurations.

Change the measurement parameter using CALCulate:PARameter:DEFine.

Relevant Modes

NA, NF

Parameters

 

<n>

Number of traces.

For NA mode, choose from 1 to 4.

For NF mode, choose from 1 to 2.

Examples

CALC:PAR:COUN 2

Query Syntax

CALCulate:PARameter:COUNt?

Default

1


Last Modified:

01june2018

Added NF mode.

15-Aug-2012

New command