DISPlay:WINDow:TRACe<n>:Y[:SCALe]:AUTO

(Write-Only) Autoscale the trace.

Relevant Modes

CAT, EMI, NA, NF, PAA, SA, FOPS

CAT mode: this command always acts on the selected trace. Select a trace using CALCulate:PARameter:SELect

SA mode: this command autoscales all displayed traces.

Parameters

 

<n>

For NA mode Only: Specify the displayed trace number. Choose from 1 to 4.

For NF mode Only: Specify the displayed trace number. Choose from 1 to 2.

If unspecified, value is set to 1.

Examples

DISPlay:WINDow:TRAC1:Y:AUTO

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

19-Mar-2014

Added FOPS

23-Jan-2013

Modified again for CAT

26-Apr-2012

Modified for CAT (5.75)