(Read-Write) Set and query the Y-axis value of the reference line. Use this command with DISPlay:WINDow:TRACe:Y[:SCALe]:RPOSition which sets the position of the reference. |
|
Relevant Modes |
CAT, EMI, NA, NF, PAA, SA, RTSA, FOPS CAT mode: This command always acts on the selected trace. Select a trace using CALCulate:PARameter:SELect SA mode: This command acts on all displayed traces. |
Parameters |
|
<n> |
NA mode Only: Specify the displayed trace number. Choose from 1 to 4. For NF mode Only: Specify the displayed trace number. Choose from 1 to 2. If unspecified, value is set to 1. |
<num> |
Y-axis reference level. Units depend on the selected format. |
Examples |
DISP:WIND:TRAC1:Y:RLEV -50 |
Query Syntax |
DISPlay:WINDow:TRACe<n>:Y[:SCALe]:RLEVel? |
Return Type |
Numeric |
Default |
Depends on Mode |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
01june2018 |
Added NF mode Opt. 356 (10.3) |
10-june-2016 |
Added RTSA mode (9.50) |
20-Mar-2014 |
Added FOPS |
23-Jan-2013 |
Modified again |
26-Apr-2012 |
Modified for CAT (5.75) |