DISPlay:WINDow:TRACe<n>:Y[:SCALe]:TOP <num>

(Read-Write) Set and query the top (upper) Y-axis scale value.

Relevant Modes

CAT, EMI, NA, NF, SA

CAT mode: this command always acts on the selected trace.

SA mode: Read ONLY

Parameters

 

<n>

NA and NF mode Only: Specify the displayed trace number.

NA: Choose from 1 to 4.

NF: Choose from 1 to 2.

If unspecified, value is set to 1.

<num>

Top scale value. Units depend on the selected format.

Examples

DISP:WIND:TRAC1:Y:TOP 0

Query Syntax

DISPlay:WINDow:TRACe<n>:Y[:SCALe]:TOP?

Return Type

Numeric

Default

Depends on Mode


Last Modified:

04no2022

Added EMI mode (12.3x)

01-june-2018

Added Opt. 356 NF(10.3)

23-Jan-2013

Modified again

26-Apr-2012

Modified for CAT (5.75)