DISPlay:WINDow[:SELect] <int>

(Read-Write) Set and query the selected trace display window. This command is used to modify existing pre-defined view, or create customized view. Window and Win State (DISP:WIND:STAT) keys are used to modify layout of view, the Data (DISP:WIND:DATA) command is used to specify the displayed data results for current window.

Relevant Modes

IQA

Parameters

 

<integer>

Choices: 1, 2, 3, or 4

Examples

DISP:WIND 3

Query Syntax

DISP:WIND?

Return Type

Integer

Default

1


Last Modified:

22oct2017

Added IQA mode (10.1x)