:DLOGging:PLAYback:POSition <num>

(Read-Write)  Set and return a component carrier position. Use this command to specify a component carrier number when playback is paused.

See also DLOGging:PLAYback:PAUSe, DLOGging:PLAYback:STARt and DLOGging:PLAYback:STOP.

Relevant Modes

CS, LTE FDD, Mapping, PAA, 5G NR, 5G NR EVM Conducted, and 5GTF

Parameters

 

<num>

Enter a value between 1 and the total recorded result:

- 10000 maximum

Examples

RECP:ACT:POS 2

Query Syntax

:RECPlayback:ACTion:POSition?

Default

1


Last Modified:

12dec2019

Added 5G NR and 5G NR EVM Conducted (A.11.5x)

01june2019

New command