(Read-Write) Set the byte order used for data transfer. This command is only implemented if FORMAT:DATA is set to :REAL. If FORMAT:DATA is set to :ASCII, the swapped command is ignored. |
|
Relevant Modes |
ALL |
Parameters |
|
<char> |
Choose from: NORMal - LSB first; for "x86 or "Little Endian" computers . SWAPped - MSB first. Use when your controller is anything other than an IBM compatible computers. Use SWAPped if you are using VEE, LabView, or T&M Tool kit. NOTE: These descriptions may be reversed from other Keysight Instruments, but compliant with IEE 488.2. SWAPed (MSB first) is very slow. |
Examples |
FORM:BORD NORM |
Query Syntax |
FORMat:BORDer? |
Default |
NORMal |
Last Modified:
31-Oct-2013 |
New command |