|
(Write-Only) Causes the FieldFox to perform a single sweep, then hold. Use this sweep mode for reading trace data. First send INIT:CONT 0 to set single sweep mode. When in Continuous sweep mode, this command is ignored. This command is overlapped. This means that it will execute and, while the FieldFox performs a single sweep, it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands. |
|
|
Relevant Modes |
ALL |
|
Examples |
INIT;*OPC? |
|
Query Syntax |
Not Applicable |
|
Default |
Not Applicable |