INITiate:CONTinuous <bool>

(Read-Write) Specify acquisition mode for the FieldFox.

The OFF setting for this command is overlapped. This means that it will execute and also accept new commands while switching to single sweep (acquisition for I/Q) mode.

Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands.

See also, INITiate:IQCapture.

Relevant Modes

ALL

Parameters

 

<boolean>

Acquisition mode. Choose from:

O or OFF - Single acquisition mode. Use INIT:IMM to trigger a acquisition.

1 or ON - Continuous acquisition mode

Examples

INIT:CONT 0;*OPC?

See example in VVM mode

Query Syntax

INITiate:CONTinuous?

Return Type

Boolean

Default

ON - Continuous


Last Modified:

22oct2017

Added IQA mode (10.1x)