INITiate:IQCapture

(Write-Only) Causes the FieldFox to start the I/Q capture process. When in Single sweep (acquisition for I/Q) mode, the IQA performs the current defined I/Q capture before going to the hold state again.

This command is overlapped. This means that it will execute and, while the FieldFox performs a single sweep (acquisition for I/Q), it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands.

Note: This command can only be used in single acquisition mode. It is ignored when the I/Q capture is set to continuous acquisition. To enable/disable continuous acquisition, refer to INITiate:CONTinuous.

Relevant Modes

IQA

Examples

INIT:IQC;*OPC?

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

13nov2017

Added IQA mode (10.1x)