(Write-only) Load a source antenna file from the specified device. To load a receiver (or only one) antenna file, use MMEMory:LOAD:ANTenna
|
|
Relevant Modes |
EMI, SA |
Parameters |
|
<string> |
For *.csv files, provide filename of the antenna file WITHOUT an extension. For *.ant files, provide filename and .ant extension. |
<char> |
Memory device where the Antenna file is stored. Choose from the following:
|
Examples |
MMEM:LOAD:SANT "MyAntenna",INT mmemory:load:santenna "demo_antenna_26m_3g.ant",internal |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
26-Jan-2015 |
New command (8.0) |