MMEMory:LOAD:ANTenna <string>,<char>

(Write-only) Load a receiver antenna file from the specified device. If using only one antenna file, use this command.

For SA (Only), to load a source antenna file, use MMEMory:LOAD:SANTenna.

  • All Channel Scanner (ChScn) PAA, and SA mode Antenna files are saved and recalled as *.csv files, which allows them to also be read by spreadsheet programs.

  • The FieldFox can also read *.ANT (Antenna) files that were created from older Keysight Spectrum Analyzers.

  • Antenna files are saved and recalled from the "Antenna" folder. If the folder does not already exist on a USB or SD card, it is created automatically before storing the file.

See ALL MMEM commands.

Relevant Modes

ChScn, EMI, PAA, SA

Parameters

 

<string>

For *.csv files, provide filename of the antenna file WITHOUT an extension.

For *.ant files, provide filename and .ant extension.

<char>

Memory device where the Antenna file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:LOAD:ANT "MyAntenna",INT

mmemory:load:antenna "demo_antenna_26m_3g.ant",internal

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

04no2022

Added EMI mode (12.3x)

01dec2019

Added PAA (11.5)

01june2018

Added Channel Scanner (ChScn) - (10.3)

26-Jan-2015

Modified for source

16-Dec-2014

Fixed .ant recall

29-Oct-2010

New command (5.30)