(Read-Write) Loads a source cable file from the specified device. To load a receiver (or only one) cable file, use MMEMory:LOAD:CABLe
|
|
Relevant Modes |
CAT, EMI, SA |
Parameters |
|
<string> |
SA mode: Filename of the cable file withOUT an extension. CAT mode: Filename of the cable file with an extension. |
<char> |
Memory device where the cable file is stored. Choose from:
|
Examples |
MMEM:LOAD:SCAB "MyCable",INT */SA mode MMEM:LOAD:SCAB "MyCable.xml",INT */CAT mode |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
27nov2-18 |
Updated filename load descriptions with mode specific content. |
26-Jan-2015 |
New command (8.00) |