(Read-Write) Loads a receiver cable file from the specified device. If using only one cable file, use this command. To load a source cable file, use MMEMory:LOAD:SCABle
|
|
Relevant Modes |
|
Parameters |
|
<string> |
SA mode: Filename of the cable file withOUT an extension. CAT mode: Filename of the cable file with an extension. |
<char> |
Memory device where the cable file is stored. Choose from:
|
Examples |
MMEM:LOAD:CABL "MyCable",INT */ChnSCn, PAA, and SA modes MMEM:LOAD:CABL "MyCable.xml",INT */CAT mode |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
27nov2-18 |
Updated filename load descriptions with mode specific content. |
01june2018 |
Added Channel Scanner (ChScn) - (10.3) |
26-Jan-2015 |
Modified for source |
29-Oct-2010 |
New command (5.30) |