(Write-only) Saves the currently-loaded receiver antenna table to a file on the specified device.
|
|
Relevant Modes |
|
Parameters |
|
<string> |
Filename of the antenna file WITHOUT an extension. |
<char> |
Memory device where the antenna file is to be stored. Choose from:
|
Examples |
MMEM:STOR:ANT "MyAntenna_1",USB |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
01dec2019 |
Added PAA (11.5) |
01june2018 |
Added Channel Scanner (ChScn) - (10.3) |
16-Dec-2014 |
Edit to *.ant files |
22-Aug-2012 |
Fixed example |
22-Oct-2010 |
New command (5.30) |