MMEMory:STORe:FDATa <filename>

(Write-only) Saves the selected formatted trace to a CSV or KML file to a default folder. (i.e., this is a screen capture from the currently displayed trace.)

See also, MMEM:STOR:MAT, MMEM:STOR:SDF, and MMEM:STOR:TXT.

Relevant Modes

 5G NR, 5G NR EVM Conducted, 5GTF, CAT, EMI, IQA, LTE FDD, PAA, NA, NF, RTSA, SA, Pulse Measurements

Parameters

 

<filename>

Filename and extension into which data will be loaded.

Examples

MMEM:STOR:FDAT "MyFile.csv"

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

04no2022

Added EMI mode (12.3x)

12dec2019

Added 5G NR and 5G NR EVM Conducted (A.11.5x)

03dec2018

Added LTE FDD & 5GTF (A.11.0)

01june2018

Added NF mode Opt. 356 (10.3)

21nov2017

Added IQA mode (A.10.15)

20-sep-2016

Added RTSA mode (A.09.50)

31-Oct-2013

Added Pulse

23-Apr-2012

Major modifications