MMEMory:STORe:SANTenna <string>,<char>

(Write-only) Load a source antenna file from the specified device.

To load a receiver (or only one) antenna file, use MMEMory:LOAD:ANTenna

  • All SA mode Antenna files are saved and recalled as *.csv files, which allows them to also be read by spreadsheet programs.

  • The FieldFox can also read *.ANT (Antenna) files that were created from older Keysight Spectrum Analyzers.

  • Antenna files are saved and recalled from the "Antenna" folder. If the folder does not already exist on a USB or SD card, it is created automatically before storing the file.

See ALL MMEM commands.

Relevant Modes

EMI, SA

Parameters

 

<string>

For *.csv files, provide filename of the antenna file WITHOUT an extension.

For *.ant files, provide filename and .ant extension.

<char>

Memory device where the Antenna file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:LOAD:SANT "MyAntenna",INT

mmemory:load:santenna "demo_antenna_26m_3g.ant",internal

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

04no2022

Added EMI mode (12.3x)

26-Jan-2015

New command (8.0)