[:SENSe]:ADEMod:METRics:FMTY <int>

(Read-Write) Set the FM window Y axis frequency value (1 kHz to 1 GHz).

See also, ADEMod:METRics:AMTY, ADEMod:METRics:PMTY, ADEMod:METRics:SSBTY and ADEMod:METRics:DTYPe

Relevant Modes

SA

Parameters

 

<num>

FM Y axis frequency

Note: This commands accepts MINimum and MAXimum commands.

Examples

ADEM:METR:FMTY 1e9 'Sets the Y Axis to the maximum of 1 GHz

ADEM:METR:FMTY MAX 'Sets the Y Axis to the maximum of 1 GHz

ADEM:METR:FMTY MIN 'Sets the Y Axis to the minimum of 1 kHz

Query Syntax

:ADEM:METR:FMTY?

Return Type

Numeric

Default

100e3 (1 kHz)


Last Modified:

16-Dec-2015

Added AM/FM Metrics (A.12.3x)