[:SENSe]:ADEMod:METRics:PMTY <int>

(Read-Write) Sets the PM window Y axis top radian value (0-100).

See also, ADEMod:METRics:AMTY, ADEMod:METRics:FMTY, ADEMod:METRics:SSBTY and ADEMod:METRics:DTYPe

Relevant Modes

SA

Parameters

 

<value>

PM Y axis percentage

Note: This commands accepts MINimum and MAXimum commands.

Examples

ADEM:METR:PMTY 10 'Sets Y axis to 10 radians

ADEM:METR:PMTY MAX 'Sets the Y axis to 100 radians

Query Syntax

:ADEM:METR:PMTY?

Return Type

Value

Default

5


Last Modified:

16-Dec-2015

Added AM/FM Metrics (A.12.3x)