This command has been replaced by [:SENSe]:ALIGnment:AMPLitude[:STATe]. Learn about superseded commands.
|
(Read-Write) Set and query the alignment amplitude (InstAlign) state. |
|
|
Relevant Modes |
IQA, SA, CPM, RTSA All models with InstAlign capability (All EXCEPT N9912A). |
|
Parameters |
|
|
<character> |
InstAlign state. Choose from: AUTO - The alignment process is performed every 300 seconds or when the temperature has changed about 1 degree. It occurs only at the beginning of a sweep and takes about 0.5 seconds to complete. HOLD - The alignment process is stopped, but the last alignment values are applied to subsequent sweeps. OFF - The alignment process is NOT performed. Only factory correction values are used. |
|
Examples |
:AMPL:ALIG HOLD |
|
Query Syntax |
:SENSe:AMPLitude:ALIGnment:STATe? |
|
Return Type |
Character |
|
Default |
AUTO |
Last Modified:
|
22-oct-2016 |
Added IQA mode and superseded note (A.010.15) |
|
20-sep-2016 |
Added RTSA mode (A.09.50) |
|
1-Apr-2014 |
Added CPM |
|
28-Mar-2013 |
Changed time from 30 to 300 secs |
|
17-Jul-2012 |
New command (6.00) |