|
(Read-Write) Set and query the Receiver Antenna Corrections ON/OFF state. If using only one antenna correction, use this command. For source antenna, use: [:SENSe]:AMPLitude:CORRections:SANTenna[:STATe] |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<bool> |
Antenna correction state. Choose from: OFF (or 0) - Antenna correction OFF. ON (or 1) - Antenna correction ON. |
|
Examples |
AMPL:CORR:ANT 1 |
|
Query Syntax |
[:SENSe]:AMPLitude:CORRections:ANTenna[:STATe]? |
|
Return Type |
Boolean |
|
Default |
OFF |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01june2018 |
Added Channel Scanner (ChScn) - (10.3) |
|
26-Jan-2015 |
Modified for Src/Rec |
|
17-Jul-2012 |
New command (6.00) |