|
(Write-only) Clears the Receiver Cable Correction table. This is the same as selecting the New softkey and then confirming “Yes” from the Edit/Save/Recall Antennas menu. If using only one cable correction, use this command. For source cable, use [:SENSe]:AMPLitude:CORRections:SCABle:DEFault |
|
|
Relevant Modes |
|
|
Parameters |
None |
|
Examples |
AMPL:CORR:CABL:DEF |
|
Query Syntax |
Not Applicable |
|
Default |
Not Applicable |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01june2018 |
Added Channel Scanner (ChScn) - (10.3) |
|
26-Jan-2015 |
Modified for Src/Rec |
|
17-Jul-2012 |
New command (6.00) |