(Read-Write) Set and query the frequency converter corrections ON/OFF state. Note: Typically this command is not required. Refer to AMPL:CORR:CONV:DEF. |
|
Relevant Modes |
|
Parameters |
|
<bool> |
Frequency converter correction state. Choose from: OFF (or 0) - Converter correction OFF. ON (or 1) - Converter correction ON. |
Examples |
AMPL:CORR:CONV 1 'Enables the default frequency converter corrections. |
Query Syntax |
[:SENSe]:AMPLitude:CORRections:CONVerter[:STATe]? |
Return Type |
Boolean |
Default |
OFF (0) |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
20apr2020 |
New command A12.00 |