[:SENSe]:AMPLitude:CORRections[:STATe] <bool> -  SUPERSEDED

(Read-Write) Set and query the Channel Scanner (ChScn) and SA mode corrections ON/OFF state.

This setting is labeled "Apply Corrections" on the FieldFox softkeys.

See all corrections commands

NOTE: Please use [:SENSe]:AMPLitude:CORRections:DISable in lieu of this superseded command.

Relevant Modes

ChScn, PAA, SA

Parameters

 

<bool>

Correction state. Choose from:

OFF (or 0) - Correction OFF.

ON (or 1) - Correction ON.

Examples

AMPL:CORR 1

Query Syntax

[:SENSe]:AMPLitude:CORRections[:STATe]?

Return Type

Boolean

Default

OFF


Last Modified:

23oct2020

Set up as Superseded command

01june2018

Added Channel Scanner (ChScn) - (10.3)

20-Oct-2010

New command (5.30)