[:SENSe]:AMPLitude:PSDFunction <bool>

(Read-Write) This command enables and disables the PSD function. The Power Spectral Density Function (PSD) Mode, mathematically calculates the PSD function measurement as a way to normalize the powers (Reference Level, Trace, Markers) as though they were made using a watts per hertz (W/Hz) bandwidth.

Relevant Modes

SA, EMI

Parameters

n/a

<boolr>

Choose from:

OFF(0) - PSD function OFF

ON (1) - PSD function ON

Examples

AMPL:PSDF ON */Enables the PSD function.

AMPL:PSDF 0 */Disables the PSD function.

Query Syntax

AMPL:PSDF?

Default

0 (OFF)


Last Modified:

19-Oct-2010

New command (~A.12.3x)