|
(Write-Only) Measures the OPEN calibration standard that is connected to the specified port. This command is overlapped. This means that it will execute and, while the FieldFox measures the cal standard, it will also accept new commands. Follow this command with *OPC? to cause the FieldFox to wait before accepting subsequent commands. |
|
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
|
Parameters |
|
|
<num> |
Port number to which the OPEN standard is connected. N9912A - Choose 1 (RF OUT) All other models - Choose 1 or 2 |
|
Examples |
CORR:COLL:OPEN 1 |
|
Query Syntax |
Not Applicable |
|
Default |
Not Applicable |
Last Modified:
|
18-Oct-2012 |
Added new models |