(Read-Write) Set and query the enable/disable state of the noise figure correction loss after the DUT. Use CORRection:LOSS:AFTer to set the correction loss level after the DUT (DUT Out). |
|
Relevant Modes |
|
Parameters |
|
<bool> |
Enable/Disable the DUT Out state. Choose from: ON (or 1) - The correction loss value stated using the CORRection:LOSS:AFTer command. OFF (or 0) -The correction loss after the DUT is disabled. |
Examples |
:CORR:LOSS:AFT:ENAB 1 correction:loss:after:enabled off |
Query Syntax |
:CORRection:LOSS:AFTer:ENABled? |
Return Type |
Boolean |
Default |
OFF |
Last Modified:
01-june-2018 |
Added Opt. 356 NF(10.3) |