(Read-Write) Set and query the amount of noise figure correction loss after the DUT input. Use CORRection:LOSS:AFTer:ENABled to set the correction loss level after the DUT input. |
|
Relevant Modes |
|
Parameters |
|
<double> |
Set the amount of noise figure loss correction after the DUT input. Choose from: -100 to 100 dB - The correction loss value stated using the CORRection:LOSS:AFTer:ENABled command. 0.00 dB - Default |
Examples |
:CORR:LOSS:AFT -15.55 |
Query Syntax |
:CORRection:LOSS:AFTer? |
Return Type |
Double |
Default |
OFF |
Last Modified:
01-june-2018 |
Added Opt. 356 NF(10.3) |