[:SENSe]:CORRection:UCALibration:CANCel

(Write-Only) Cancels the user calibration.

See also, [:SENSe]:CORRection:UCALibration:RUN, [:SENSe]:CORRection:RCALibration:RUN, [:SENSe]:CORRection:RCALibration:CANCel, [:SENSe]:CORRection:UCALibration:INTerpolated?, [:SENSe]:CORRection:ENR:EXTRapolated?, [:SENSe]:CORRection:UCALibration[:STATe], and [:SENSe]:CORRection:RCALibration[:STATe]?.

Note: You can use the IEEE command *.OPC? to query the status of your calibrations.

Relevant Modes

NF

Parameters

 

<not applicable>

 

Examples

CORR:UCAL:CALC 'Cancels the user calibration, when a SCPI is used to run the User calibration.

Query Syntax

no query

Return Type

not applicable

Default

not applicable


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)